Hi there,
C5515
aer_c55l_cpuv3.3_obj_17_0_0_0
volib_C55_CPU3_2_1_0_1
CCS v5.5
I have some general questions:
1. Are there any specific requirements for AER modules and buffers to be allocated into the memory? I looked through the linker file in AER demo project and realized that every module as well as buffer is allocated quite specifically. However, there is no any reference in AER documentation. Should I follow the demo or I can do it in my own way?
2. ECU package from VoLIB requires specific allocation otherwise it just does not work. I found this feature by chance moving stuff around the memory. Are the any recommendation here? All ECU Data Memory Requirements I fulfilled but it does not matter. It depends on linker file. For example, in my case ECU works when
.text: {} > SAMEM4 PAGE 0 and nothing more in SAMEM4
Thanks