We are working with a TMS320C5535 DSP on a custom board that is laid out to use the SPI, UART and GPIO on the parallel port pins. This requires us to select PPMODE1 in the EBSR register. However, when doing this we are unable to trigger receive interrupts on the UART peripheral. When placing the parallel port pins in either mux mode 5 or 6 these interrupts work as expected. I've noticed a similar issue here: https://e2e.ti.com/support/dsp/c5000/f/109/t/152927 (however, I am able to send data).
When in Mux Mode 1 I see that the registers are being set correctly (e.g., IFR bit 6 is 1, IIR sees a receive line status interrupt and there is data on the receive register) however it appears the processor never jumps to the interrupt vector. These same registers are set when in Mux Mode 5 or 6, and the PC jumps to the appropriate interrupt vector.
Is there any known issues or oddities that are known with running UART in that EBSR configuration? I was unable to find any hints in the datasheet, TRM or errata. The forums also do not seem to give any solutions (although the do mention the issue in a couple threads).