Tool/software: Code Composer Studio
Dear All,
Presently, I am working on the the project related to the implementation of parametric loudspeakers. In this project I want to generate the carrier signal of 40 KHz and modulate the audio signal onto this carrier. For this, I am using TMS320c5505 EVM and referring to the C5000 Teaching ROM available at http://processors.wiki.ti.com/index.php/Porting_C5000_Teaching_ROM_to_C5535_eZdsp . Regarding this, I have two doubts.
1) In chapter 4 of this CD-ROM, the code to generate the sinewave is given. However, using this code I can only generate the sinewave with frequency ~20 KHz. As I suggested earlier, I need to generate the sinewave with ~40 kHz. Can anyone please suggest me that how may I modify the code of chapter 4 to get the sinewave of ~40 kHz.
2) Also, how the sampling frequency can be increased to 192 Khz. I believe this is the maximum sampling frequency for TMS320c5505 EVM.
I would be really grateful if anyone could suggest me about this.
Thanks and regards,
Satyajit