Tool/software: Code Composer Studio
Hi there,
what happen if I create a bin file containing a struct variable and then I use it on a C5517 device?
My goal is to create a bin file containing a vector, then copy the file to an EPROM and then read the vector back from a C5517 device (EMIF intarface to the EPROM).
Are there incompatibilities due to the compilator?
Let' say I have this vector:
Uint16 Buffer[10] = {0,1,2,3,4,5,6,7,8,9};
Then I create a bin file with the Buffer vector.
Once I write it to an EPROM and I point to it with EMIF, will I be able to directly read Buffer[0]?
Thanks