We try to connect Emulator to C6474 with the 14 PIN JTAG.
The error imformation is as follow: (1), The emulator can be connected to C6474, the program(*.out) can be loaded to C6474, But when the program run a few seconds or a few miniutes, It will appear the following error imformation: Power Failure on Target CPU
Failed to remove the debug state from the target before disconnecting.
There may still be breakpoint opcodes embedded in program memory.
It is recommended that you reset the emulator before you connect and reload your program before you continue debugging. Power Failure on Target CPU
Failed to remove the debug state from the target before disconnecting.
There may still be breakpoint opcodes embedded in program memory.
It is recommended that you reset the emulator before you connect and reload your program before you continue debugging. (2), When we unconnect to C6474 and then reconnect the C6474, sometimes, error appears as follow: Trouble Reading Memory Block at 0x800000 on Page 0 of Length 0x2c0: Error 0x00000002/-1139 Error during: Memory,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Trouble Reading Memory Block at 0x800000 on Page 0 of Length 0x680: Error 0x00000002/-1139 Error during: Memory,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Trouble Writing Memory Block at 0x29a017c on Page 0 of Length 0x4: Error 0x00000002/-1139 Error during: Memory,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Error connecting to the target: Error 0x80000260/-1198 Fatal Error during: Execution, Initialization, OCS,
Cannot get ownership of the EXE unit.
Board Name: C6474 XDS560 Emulator, 20-pin JTAG Cable Cpu Name: C6400PLUS_0 Abort:
Close Code Composer Studio. Retry:
Try to connect to the target again. Cancel:
Remain disconnected from the target Diagnostic:
Run diagnostic utility. (3), Sometimes, The
emulator can be connected to C6474, but the program(*.out) can't be loaded to
C6474, It
will appear the following error imformation: Trouble Reading Memory Block at 0x800000 on Page 0 of Length 0x680: Error 0x00000002/-1139 Error during: Memory,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Trouble Writing Memory Block at 0x808520 on Page 0 of Length 0x6ee0: Error 0x00000006/-1139 Error during: Memory, Register,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Trouble Writing Memory Block at 0x1848200 on Page 0 of Length 0x40: Error 0x00000002/-1139 Error during: Memory,
Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR.
This will disconnect each target from the emulator.
The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. (3), Sometimes, The
emulator can be connected to C6474, but the program(*.out) can't be loaded to
C6474, It
will appear another kinds of error imformation: data verification failed at address 0813400. please verify target memory and memory map. When this kind of error appear, we have to restart the CCS program. Following is some imfortion about our the platform.
But the blackhawk emulator is hard to connect.
The xds560 sometimes can be connected.
4. Latesr CCS SR release that can support C6474.
5. Correct CCS configuration of your board.
Do you mean we need some special configuration on CCS when emulating the board?
In fact, we found some errors in the gel file, and we correct it, but it seems no use.
Do it need different emulation methods when emulating the 6474 as it has three cores?
We have tried C6474 XDS560 Emulator, 20-pin JTAG Cable configuration on XDS560 Emulator.
We also tried Blackhawk USB560m- C6474 Emulator, 20-pin JTAG Cable on Blackhawk USB560 Emulator.
The configuration all come from the Available Factory Boards on CCS.
7. Correct memory map file.
We had done some changes, but it did not work.
The gel file we have is on the attachment.
evmc6474.gel is the original gel from spectrum.3757.c6474_gel.zip
evmc6474_0.gel is changed by ourselves.
evmc6474_0.gel run longer time than evmc6474.gel.