Hi,
I have a TMS320C6670 DSP evaluation board (which doesn't have an internal ADC) and I need to interface an external ADC to it. My requirements are as follows:
I need at least 4 channels on the ADC where I will input 20-30 Khz four analog signals (having peak voltages around 1 V). The important criteria is to have simultaneous sampling and the sampling rate should be atleast 250 kSPS for each channel.
I can select the ADC but I am a bit confused for interfacing that ADC to DSP. Can anyone suggest an appropriate protocol (or a ADC evaluation board) for sending the ADC data to the mentioned DSP at higher rates so as to compensate the higher sampling rates?