Hello
some problems of NDK:
1. At the first time system starts , sometimes my NDK will work and response to ping command, but sometimes
my NDK will not work and doesn't response to ping command. I used wireshark to check the ethernet packet, and it showed that PC is sending ARP request repeatedly but NDK doesn't response at all.
2. Sometimes NDK starts working, and the TCP communication between PC and NDK works well. But if PC stops TCP communication for a while, and than PC try to start another TCP connection again, NDK failed to response. No communication between PC and NDK is possible after that point.
I don't known why sometimes NDK works but sometimes NDK doesn' t work.
my platform:
C6474, NDK 2.1.0
L2 cache: 32K