This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: Repeated on/off test

Part Number: LM5117

Hello all,

operating conditions:

Vin=50V,Vout=24V

First normal start, about 1-2s once repeated switch unable to start. At this time, the input voltage drops to about 26V.

Schematic:

Waveform:

Yellow channel output voltage
Blue channel input voltage
The green channel is driven by the lower tube. When the input voltage drops to about 26V, it will be powered on again, and it will not work.
When it not work, re-power on, measure UVLO voltage about 2.3V, VCC 7.4V, SS 4.7V or so

What could be the cause of this?