Hi,
We are using "C6678_Power_Consumption_Summary_Rev1_0_3.xlsm" to estimate power needed.
We notice that with same parameters there is about 70% increase in Core power (CVDD) when Core frequency increases from 1.0GHz to 1.25GHz.
We notice that with same parameters there is about 18% increase in Core power (CVDD) when Core frequency increases from 0.8GHz to 1.0GHz.
Is this normal? Is there a problem in the spreadsheet?
Please see below:
800MHz:
1000MHz:
1250MHz: