Hi:
I am testing the SRIO between TMX320C6678L and FPGA (ML605).
I followed the example code and set the parameters, the port initialized OK and no errors.
C:\Texas Instruments\pdk_C6678_1_0_0_16\packages\ti\drv\srio\example\SRIOLoopbackDioIsr\loopbackDioIsr.c
In the test program, in function dioSocketsWithISR(), I write 128 bytes to FPGA with SRIO NWRITE_R operation and read them back with the SRIO Read operation.
By using the chipscope in the FPGA side, I can see the data are written into the block ram of SRIO IP when the NWRITE_R command is performed, and the data are read out from the block ram of SRIO IP when the Read command is performed. I think the SRIO IP of FPGA is work correctly, however, I cannot see the data read from the FPGA to be written into the C6678 DSP's memory buffer.
Can someone give me any idea how to debug this situation, thanks.
1. The captured waveform from chipscope of SRIO IP in FPGA side. The read out data is correct.
2. After perform the Read operation, the memory is unchanged even the SRIO IP return the correct data.
3. the source code
/** * @file loopbackDioIsr.c * * @brief * This is an example application which shows how DIO transfer * completion interrupts can be registered and serviced. * * \par * NOTE: * (C) Copyright 2011 Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par*/#include <xdc/std.h>#include <string.h>#include <c6x.h>#include <xdc/runtime/IHeap.h>#include <xdc/runtime/System.h>#include <xdc/runtime/Error.h>#include <xdc/runtime/Memory.h> #include <ti/sysbios/BIOS.h>#include <ti/sysbios/knl/Task.h>#include <ti/sysbios/heaps/HeapBuf.h>#include <ti/sysbios/heaps/HeapMem.h>#include <ti/sysbios/family/c64p/Hwi.h>#include <ti/sysbios/family/c64p/EventCombiner.h> #include <ti/sysbios/family/c66/tci66xx/CpIntc.h>
/* IPC includes */ #include <ti/ipc/GateMP.h>#include <ti/ipc/Ipc.h>#include <ti/ipc/ListMP.h>#include <ti/ipc/SharedRegion.h>#include <ti/ipc/MultiProc.h>
#include <xdc/cfg/global.h>
/* SRIO Driver Include File. */#include <ti/drv/srio/srio_drv.h>#include <ti/drv/srio/srio_osal.h>
/* CPPI/QMSS Include Files. */#include <ti/drv/cppi/cppi_drv.h>#include <ti/drv/qmss/qmss_drv.h>#include <ti/drv/qmss/qmss_firmware.h>
/* CSL Chip Functional Layer */#include <ti/csl/csl_chip.h>
/* CSL Cache Functional Layer */#include <ti/csl/csl_cacheAux.h>
/* PSC CSL Include Files */#include <ti/csl/csl_psc.h>#include <ti/csl/csl_pscAux.h>
/* CSL SRIO Functional Layer */#include <ti/csl/csl_srio.h>#include <ti/csl/csl_srioAux.h>
/* CSL CPINTC Include Files. */#include<ti/csl/csl_cpIntc.h>
/********************************************************************** ************************** LOCAL Definitions ************************* **********************************************************************/
/* This is the Number of host descriptors which are available & configured * in the memory region for this example. */#define NUM_HOST_DESC 128
/* This is the size of each descriptor. */#define SIZE_HOST_DESC 48
/* MTU of the SRIO Driver. We are currently operating @ MTU of 256 bytes. */#define SRIO_MAX_MTU 256
/* This is the size of the data buffer which is used for DIO Sockets. */#define SIZE_DIO_PACKET 128
/* Defines the core number responsible for system initialization. */#define CORE_SYS_INIT 0
/* Defines number of DIO sockets used in this example */#define SRIO_DIO_LSU_ISR_NUM_SOCKETS 3
/* Defines number of transfers done by DIO sockets in this example */#define SRIO_DIO_LSU_ISR_NUM_TRANSFERS 3
/* ISR timeout value (in cycles) used in this example */#define SRIO_DIO_LSU_ISR_TIMEOUT 50000
#define DST ((Uint8 *)0x100000)
/********************************************************************** ************************** Global Variables ************************** **********************************************************************/
/* Memory allocated for the descriptors. This is 16 bit aligned. */#pragma DATA_ALIGN (host_region, 16)Uint8 host_region[NUM_HOST_DESC * SIZE_HOST_DESC];
/* Memory used for the accumulator list. */#pragma DATA_ALIGN (gHiPriAccumList, 16)UInt32 gHiPriAccumList[64];
/* Global SRIO and QMSS Configuration */Qmss_InitCfg qmssInitConfig;
/* Global Varialble which keeps track of the core number executing the * application. */UInt32 coreNum = 0xFFFF;
/* Shared Memory Variable to ensure synchronizing SRIO initialization * with all the other cores. */#pragma DATA_ALIGN (isSRIOInitialized, 128)#pragma DATA_SECTION (isSRIOInitialized, ".srioSharedMem");volatile Uint32 isSRIOInitialized = 0;
Srio_DrvHandle hAppManagedSrioDrv;Srio_DrvHandle hDrvManagedSrioDrv;
CSL_SrioHandle hSrioCSL;
/* These are the device identifiers used in the Example Application */const uint32_t DEVICE_ID1_16BIT = 0xBEEF;const uint32_t DEVICE_ID1_8BIT = 0xAB;const uint32_t DEVICE_ID2_16BIT = 0x4560;const uint32_t DEVICE_ID2_8BIT = 0xCD;const uint32_t DEVICE_ID3_16BIT = 0x1234;const uint32_t DEVICE_ID3_8BIT = 0x12;//const uint32_t DEVICE_ID4_16BIT = 0x5678;const uint32_t DEVICE_ID4_16BIT = 0xABFF;const uint32_t DEVICE_ID4_8BIT = 0x56;
/* Array containing SRIO socket handles */Srio_SockHandle srioSocket[SRIO_DIO_LSU_ISR_NUM_SOCKETS];
/* Source and Destination Data Buffers (payload buffers) */UInt8* srcDataBuffer[SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS];UInt8* dstDataBuffer[SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS];
/* Global debug variable to track number of ISRs raised */volatile UInt32 srioDbgDioIsrCnt = 0;
/* Global variable to indicate completion of ISR processing */volatile UInt32 srioLsuIsrServiced = 0;
/* Global variables to count good and bad transfers */volatile UInt32 srioDioLsuGoodTransfers = 0;volatile UInt32 srioDioLsuBadTransfers = 0;
/********************************************************************** ************************* Extern Definitions ************************* **********************************************************************/
extern UInt32 malloc_counter;extern UInt32 free_counter;
extern int32_t SrioDevice_init (void);
/* QMSS device specific configuration */extern Qmss_GlobalConfigParams qmssGblCfgParams;
/* CPPI device specific configuration */extern Cppi_GlobalConfigParams cppiGblCfgParams;
/* OSAL Data Buffer Memory Initialization. */extern int32_t Osal_dataBufferInitMemory(uint32_t dataBufferSize);
/********************************************************************** ************************ SRIO EXAMPLE FUNCTIONS ********************** **********************************************************************/
/** * @b Description * @n * Utility function which converts a local address to global. * * @param[in] addr * Local address to be converted * * @retval * Global Address */static UInt32 l2_global_address (Uint32 addr){ UInt32 corenum;
/* Get the core number. */ corenum = CSL_chipReadReg(CSL_CHIP_DNUM);
/* Compute the global address. */ return (addr + (0x10000000 + (corenum*0x1000000)));}
/** * @b Description * @n * Utility function that is required by the IPC module to set the proc Id. * The proc Id is set via this function instead of hard coding it in the .cfg file * * @retval * Not Applicable. */Void myStartupFxn (Void){ MultiProc_setLocalId (CSL_chipReadReg (CSL_CHIP_DNUM));}
/** * @b Description * @n * This function enables the power/clock domains for SRIO. * * @retval * Not Applicable. */static Int32 enable_srio (void){#ifndef SIMULATOR_SUPPORT /* SRIO power domain is turned OFF by default. It needs to be turned on before doing any * SRIO device register access. This not required for the simulator. */
/* Set SRIO Power domain to ON */ CSL_PSC_enablePowerDomain (CSL_PSC_PD_SRIO);
/* Enable the clocks too for SRIO */ CSL_PSC_setModuleNextState (CSL_PSC_LPSC_SRIO, PSC_MODSTATE_ENABLE);
/* Start the state transition */ CSL_PSC_startStateTransition (CSL_PSC_PD_SRIO);
/* Wait until the state transition process is completed. */ while (!CSL_PSC_isStateTransitionDone (CSL_PSC_PD_SRIO));
/* Return SRIO PSC status */ if ((CSL_PSC_getPowerDomainState(CSL_PSC_PD_SRIO) == PSC_PDSTATE_ON) && (CSL_PSC_getModuleState (CSL_PSC_LPSC_SRIO) == PSC_MODSTATE_ENABLE)) { /* SRIO ON. Ready for use */ return 0; } else { /* SRIO Power on failed. Return error */ return -1; }#else /* PSC is not supported on simulator. Return success always */ return 0;#endif}
/** * @b Description * @n * This function is application registered SRIO DIO LSU interrupt * handler (ISR) which is used to process the pending DIO Interrupts. * SRIO Driver users need to ensure that this ISR is plugged with * their OS Interrupt Management API. The function expects the * Interrupt Destination information to be passed along to the * API because the DIO interrupt destination mapping is configurable * during SRIO device initialization. * * @param[in] argument * SRIO Driver Handle * * @retval * Not Applicable */static void myDioTxCompletionIsr ( UArg argument){ /* Pass the control to the driver DIO Tx Completion ISR handler */ Srio_dioTxCompletionIsr ((Srio_DrvHandle)argument, hSrioCSL);
/* Wake up the pending task */ srioLsuIsrServiced = 1;
/* Debug: Increment the ISR count */ srioDbgDioIsrCnt++;
return;}
/** * @b Description * @n * The function demonstrates usage of interrupts to indicate * the end of DIO transfers * * @param[in] hSrioDrv * Handle to the SRIO driver * * @retval * Success - 0 * @retval * Error - <0 */static Int32 dioSocketsWithISR (Srio_DrvHandle hSrioDrv, uint8_t dio_ftype, uint8_t dio_ttype){ Srio_SockBindAddrInfo bindInfo; Srio_SockAddrInfo to; uint16_t sockIdx, i, compCode; uint16_t counter, srcDstBufIdx = 0; int32_t eventId, startTime; UInt8 **srcDataBufPtr = NULL, **dstDataBufPtr = NULL;
System_printf ("*************************************************************\n"); System_printf ("******* DIO Socket Example with Interrupts (Core %d) ********\n", coreNum); System_printf ("*************************************************************\n");
/* Get the CSL SRIO Handle. */ hSrioCSL = CSL_SRIO_Open (0); if (hSrioCSL == NULL) return -1;
/* SRIO DIO Interrupts need to be routed from the CPINTC0 to GEM Event. * - We have configured DIO Interrupts to get routed to Interrupt Destination 0 * (Refer to the CSL_SRIO_RouteLSUInterrupts API configuration in the SRIO Initialization) * - We want this System Interrupt to mapped to Host Interrupt 8 */
/* Disable Interrupt Pacing for INTDST0 */ CSL_SRIO_DisableInterruptPacing (hSrioCSL, 0);
/* Route LSU0 ICR0 to INTDST0 */ CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 0, 0);
/* Route LSU0 ICR1 to INTDST0 */ CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 1, 0);
/* Route LSU0 ICR2 to INTDST0 */ CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 2, 0);
/* Map the System Interrupt i.e. the Interrupt Destination 0 interrupt to the DIO ISR Handler. */ CpIntc_dispatchPlug(CSL_INTC0_INTDST0, (CpIntc_FuncPtr)myDioTxCompletionIsr, (UArg)hSrioDrv, TRUE);
/* The configuration is for CPINTC0. We map system interrupt 112 to Host Interrupt 8. */ CpIntc_mapSysIntToHostInt(0, CSL_INTC0_INTDST0, 8);
/* Enable the Host Interrupt. */ CpIntc_enableHostInt(0, 8);
/* Enable the System Interrupt */ CpIntc_enableSysInt(0, CSL_INTC0_INTDST0);
/* Get the event id associated with the host interrupt. */ eventId = CpIntc_getEventId(8);
/* Plug the CPINTC Dispatcher. */ EventCombiner_dispatchPlug (eventId, CpIntc_dispatch, 8, TRUE);
for (sockIdx = 0; sockIdx < SRIO_DIO_LSU_ISR_NUM_SOCKETS; sockIdx++) { /* Open DIO SRIO Non-Blocking Socket */ srioSocket[sockIdx] = Srio_sockOpen (hSrioDrv, Srio_SocketType_DIO, FALSE); if (srioSocket[sockIdx] == NULL) { System_printf ("Error: Unable to open the DIO socket - %d\n", sockIdx); return -1; }
/* DIO Binding Information: Use 16 bit identifiers and we are bound to the first source id. * and we are using 16 bit device identifiers. */ bindInfo.dio.doorbellValid = 0; bindInfo.dio.intrRequest = 1; bindInfo.dio.supInt = 0; bindInfo.dio.xambs = 0; bindInfo.dio.priority = 0; bindInfo.dio.outPortID = 0; bindInfo.dio.idSize = 1; bindInfo.dio.srcIDMap = sockIdx; bindInfo.dio.hopCount = 0; bindInfo.dio.doorbellReg = 0; bindInfo.dio.doorbellBit = 0;
/* Bind the SRIO socket: DIO sockets do not need any binding information. */ if (Srio_sockBind_DIO (srioSocket[sockIdx], &bindInfo) < 0) { System_printf ("Error: Binding the SIO socket failed.\n"); return -1; } }
/* Allocate memory for the Source and Destination Buffers */ for (i = 0; i < (SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS); i++) { srcDataBuffer[i] = (uint8_t*)Osal_srioDataBufferMalloc(SIZE_DIO_PACKET); if (srcDataBuffer[i] == NULL) { System_printf ("Error: Source Buffer (%d) Memory Allocation Failed\n", i); return -1; } dstDataBuffer[i] = (uint8_t*)Osal_srioDataBufferMalloc(SIZE_DIO_PACKET); if (dstDataBuffer[i] == NULL) { System_printf ("Error: Destination Buffer (%d) Memory Allocation Failed\n", i); return -1; }
/* Initialize the data buffers */ for (counter = 0; counter < SIZE_DIO_PACKET; counter++) { srcDataBuffer[i][counter] = counter + (i * 5); dstDataBuffer[i][counter] = 0; } /* Debug Message: */ System_printf ("Debug(Core %d): Starting the DIO Data Transfer - Src(%d) 0x%p Dst(%d) 0x%p\n", coreNum, i, srcDataBuffer[i], i, dstDataBuffer[i]); }
if ((dio_ftype == Srio_Ftype_WRITE) && (dio_ttype == Srio_Ttype_Write_NWRITE_R)) { /* DIO Write operation */ srcDataBufPtr = &srcDataBuffer[0]; dstDataBufPtr = &dstDataBuffer[0]; } else if ((dio_ftype == Srio_Ftype_REQUEST) && (dio_ttype == Srio_Ttype_Request_NREAD)) { /* DIO Read operation */ srcDataBufPtr = &dstDataBuffer[0]; dstDataBufPtr = &srcDataBuffer[0]; } else { /* Debug Message: */ System_printf ("Debug(Core %d): Unexpected combination of FTYPE and TTYPE. Example couldn't run. Exiting!!!\n", coreNum); return -1; }
/********************************************************************************* * Run multiple iterations of the example to ensure multiple data transfers work *********************************************************************************/ for (counter = 0; counter < SRIO_DIO_LSU_ISR_NUM_TRANSFERS; counter++) { for (sockIdx = 0; sockIdx < SRIO_DIO_LSU_ISR_NUM_SOCKETS; sockIdx++) { /* Populate the DIO Address Information where the data is to be sent. */ to.dio.rapidIOMSB = 0x0; to.dio.rapidIOLSB = (uint32_t)DST; to.dio.dstID = DEVICE_ID4_16BIT; to.dio.ttype = dio_ttype; to.dio.ftype = dio_ftype;
/* Send the DIO Information. */ if (Srio_sockSend_DIO (srioSocket[0], srcDataBufPtr[0], SIZE_DIO_PACKET, (Srio_SockAddrInfo*)&to) < 0) { System_printf ("Debug(Core %d): DIO Socket Example Failed\n", coreNum); return -1; }
System_printf("RapidIO Address LSB=%x\n", hSrioCSL->LSU_CMD->RIO_LSU_REG1); System_printf("DSP Address=%x\n", hSrioCSL->LSU_CMD->RIO_LSU_REG2); System_printf("byte count=%d\n", hSrioCSL->LSU_CMD->RIO_LSU_REG3); System_printf("RIO_LSU_REG4=%x\n", hSrioCSL->LSU_CMD->RIO_LSU_REG4); System_printf("type=%x\n", hSrioCSL->LSU_CMD->RIO_LSU_REG5);
/* Wait for the interrupt to occur without touching the peripheral. */ /* Other useful work could be done here such as by invoking a scheduler */ startTime = TSCL; while((! srioLsuIsrServiced) && ((TSCL - startTime) < SRIO_DIO_LSU_ISR_TIMEOUT));
if (! srioLsuIsrServiced) { System_printf ("ISR didn't happen within set time - %d cycles. Example failed !!!\n", SRIO_DIO_LSU_ISR_TIMEOUT); return -1; }
/* Debug Message: Data Transfer was completed successfully. */ System_printf ("Debug(Core %d): DIO Socket (%d) Send for iteration %d\n", coreNum, sockIdx, counter);
/* Read the completion code filled by the ISR */ compCode = 0xFF; if (Srio_getSockOpt(srioSocket[sockIdx], Srio_Opt_DIO_READ_SOCK_COMP_CODE, &compCode, sizeof(uint8_t)) < 0) { System_printf ("Error: Unable to read the completion code in socket\n"); return -1; } /* Was the transfer good. */ if (compCode == 0) { srioDioLsuGoodTransfers++; } else { srioDioLsuBadTransfers++; }
/* Clear the LSU pending interrupt (ICCx) */ CSL_SRIO_ClearLSUPendingInterrupt (hSrioCSL, 0xFFFFFFFF, 0xFFFFFFFF); srioLsuIsrServiced = 0; /* Debug Message: Display ISR count */ System_printf ("Debug(Core %d): ISR Count: %d\n", coreNum, srioDbgDioIsrCnt);
/* Load next set of payload buffers */ srcDstBufIdx++; if (srcDstBufIdx > (SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS)) { System_printf ("Debug(Core %d): DIO Socket Example --- Out of SRC and DST buffers\n", coreNum); return -1; } } }
/********************************************************************************* * Run multiple iterations of the example to ensure multiple data transfers work *********************************************************************************/ srcDstBufIdx=0;
for (counter = 0; counter < SRIO_DIO_LSU_ISR_NUM_TRANSFERS; counter++) { for (sockIdx = 0; sockIdx < SRIO_DIO_LSU_ISR_NUM_SOCKETS; sockIdx++) { /* Populate the DIO Address Information where the data is to be sent. */ to.dio.rapidIOMSB = 0x0; to.dio.rapidIOLSB = (uint32_t)DST; to.dio.dstID = DEVICE_ID4_16BIT; to.dio.ttype = Srio_Ttype_Request_NREAD; to.dio.ftype = Srio_Ftype_REQUEST;
/* Send the DIO Information. */ if (Srio_sockSend_DIO (srioSocket[0], dstDataBufPtr[0], SIZE_DIO_PACKET, (Srio_SockAddrInfo*)&to) < 0) { System_printf ("Debug(Core %d): DIO Socket Example Failed\n", coreNum); return -1; }
// Validate the received buffer. for (i = 0; i < (SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS); i++) { for (counter = 0; counter < SIZE_DIO_PACKET; counter++) { if (dstDataBufPtr[i][counter] != srcDataBufPtr[i][counter]) { System_printf ("Error(Core %d): Data Validation error. Buffer Number (%d): Expected 0x%x got 0x%x @ index %d\n", coreNum, i, srcDataBufPtr[i][counter], dstDataBufPtr[i][counter], counter); return -1; } } }
// Debug Message: Print error counters // System_printf ("Debug(Core %d): Transfer Completion without Errors - %d\n", coreNum, srioDioLsuGoodTransfers); System_printf ("Debug(Core %d): Transfer Completion with Errors - %d\n", coreNum, srioDioLsuBadTransfers);
// Debug Message: Data was validated // System_printf ("Debug(Core %d): DIO Transfer Data Validated for all iterations\n", coreNum);
// Cleanup the source & destination buffers. // for (srcDstBufIdx = 0; srcDstBufIdx < (SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS); srcDstBufIdx++) { Osal_srioDataBufferFree ((Void*)srcDataBufPtr[srcDstBufIdx], SIZE_DIO_PACKET); Osal_srioDataBufferFree ((Void*)dstDataBufPtr[srcDstBufIdx], SIZE_DIO_PACKET); }
// Close the sockets // for (sockIdx = 0; sockIdx < SRIO_DIO_LSU_ISR_NUM_SOCKETS; sockIdx++) { Srio_sockClose_DIO (srioSocket[sockIdx]); }
// Debug Message: Example completed // if ((dio_ftype == Srio_Ftype_WRITE) && (dio_ttype == Srio_Ttype_Write_NWRITE_R)) { System_printf ("Debug(Core %d): DIO Data Transfer (WRITE) with Interrupts Example Passed\n", coreNum); } else if ((dio_ftype == Srio_Ftype_REQUEST) && (dio_ttype == Srio_Ttype_Request_NREAD)) { System_printf ("Debug(Core %d): DIO Data Transfer (READ) with Interrupts Example Passed\n", coreNum); }
return 0;}
static Int32 dioSocketsWithISR_Write (Srio_DrvHandle hSrioDrv, uint8_t dio_ftype, uint8_t dio_ttype){ Srio_SockBindAddrInfo bindInfo; Srio_SockAddrInfo to; uint16_t sockIdx, i, compCode; uint16_t counter, srcDstBufIdx = 0; int32_t eventId, startTime; UInt8 **srcDataBufPtr = NULL, **dstDataBufPtr = NULL;
static Int32 dioSocketsWithISR_Read (Srio_DrvHandle hSrioDrv, uint8_t dio_ftype, uint8_t dio_ttype){ Srio_SockBindAddrInfo bindInfo; Srio_SockAddrInfo to; uint16_t sockIdx, i, compCode; uint16_t counter, srcDstBufIdx = 0; int32_t eventId, startTime; UInt8 **srcDataBufPtr = NULL, **dstDataBufPtr = NULL; System_printf ("*************************************************************\n"); System_printf ("******* DIO Socket Example with Interrupts (Core %d) ********\n", coreNum); System_printf ("*************************************************************\n");
/* Initialize the data buffers */ for (counter = 0; counter < SIZE_DIO_PACKET; counter++) { srcDataBuffer[i][counter] = 0xff; dstDataBuffer[i][counter] = 0xff; } /* Debug Message: */ System_printf ("Debug(Core %d): Starting the DIO Data Transfer - Src(%d) 0x%p Dst(%d) 0x%p\n", coreNum, i, srcDataBuffer[i], i, dstDataBuffer[i]); } if ((dio_ftype == Srio_Ftype_WRITE) && (dio_ttype == Srio_Ttype_Write_NWRITE_R)) { /* DIO Write operation */ srcDataBufPtr = &srcDataBuffer[0]; dstDataBufPtr = &dstDataBuffer[0]; } else if ((dio_ftype == Srio_Ftype_REQUEST) && (dio_ttype == Srio_Ttype_Request_NREAD)) { /* DIO Read operation */ srcDataBufPtr = &dstDataBuffer[0]; dstDataBufPtr = &srcDataBuffer[0]; } else { /* Debug Message: */ System_printf ("Debug(Core %d): Unexpected combination of FTYPE and TTYPE. Example couldn't run. Exiting!!!\n", coreNum); return -1; }
//for (i=0; i<40; i++) /* Send the DIO Information. */ if (Srio_sockSend_DIO (srioSocket[0], srcDataBufPtr[0], SIZE_DIO_PACKET, (Srio_SockAddrInfo*)&to) < 0) { System_printf ("Debug(Core %d): DIO Socket Example Failed\n", coreNum); return -1; }
/* Read the completion code filled by the ISR */ compCode = 0xFF; if (Srio_getSockOpt(srioSocket[0], Srio_Opt_DIO_READ_SOCK_COMP_CODE, &compCode, sizeof(uint8_t)) < 0) { System_printf ("Error: Unable to read the completion code in socket\n"); return -1; } /* Was the transfer good. */ if (compCode == 0) { srioDioLsuGoodTransfers++; } else { srioDioLsuBadTransfers++; }
// Cleanup the source & destination buffers. // for (srcDstBufIdx = 0; srcDstBufIdx < (SRIO_DIO_LSU_ISR_NUM_SOCKETS * SRIO_DIO_LSU_ISR_NUM_TRANSFERS); srcDstBufIdx++) { Osal_srioDataBufferFree ((Void*)srcDataBufPtr[srcDstBufIdx], SIZE_DIO_PACKET); Osal_srioDataBufferFree ((Void*)dstDataBufPtr[srcDstBufIdx], SIZE_DIO_PACKET); } // Close the sockets // for (sockIdx = 0; sockIdx < SRIO_DIO_LSU_ISR_NUM_SOCKETS; sockIdx++) { Srio_sockClose_DIO (srioSocket[sockIdx]); }
/** * @b Description * @n * System Initialization Code. This is added here only for illustrative * purposes and needs to be invoked once during initialization at * system startup. * * @retval * Success - 0 * @retval * Error - <0 */static Int32 system_init (Void){ Int32 result; Qmss_MemRegInfo memRegInfo;
/* Initialize the QMSS Configuration block. */ memset (&qmssInitConfig, 0, sizeof (Qmss_InitCfg)); /* Initialize the Host Region. */ memset ((void *)&host_region, 0, sizeof(host_region));
/* Set up the linking RAM. Use the internal Linking RAM. * LLD will configure the internal linking RAM address and maximum internal linking RAM size if * a value of zero is specified. Linking RAM1 is not used */ qmssInitConfig.linkingRAM0Base = 0; qmssInitConfig.linkingRAM0Size = 0; qmssInitConfig.linkingRAM1Base = 0; qmssInitConfig.maxDescNum = NUM_HOST_DESC;
#ifdef xdc_target__bigEndian /* PDSP Configuration: Big Endian */ qmssInitConfig.pdspFirmware[0].pdspId = Qmss_PdspId_PDSP1; qmssInitConfig.pdspFirmware[0].firmware = &acc48_be; qmssInitConfig.pdspFirmware[0].size = sizeof (acc48_be);#else /* PDSP Configuration: Little Endian */ qmssInitConfig.pdspFirmware[0].pdspId = Qmss_PdspId_PDSP1; qmssInitConfig.pdspFirmware[0].firmware = &acc48_le; qmssInitConfig.pdspFirmware[0].size = sizeof (acc48_le);#endif
/* Initialize Queue Manager Sub System */ result = Qmss_init (&qmssInitConfig, &qmssGblCfgParams); if (result != QMSS_SOK) { System_printf ("Error initializing Queue Manager SubSystem error code : %d\n", result); return -1; }
/* Start the QMSS. */ if (Qmss_start() != QMSS_SOK) { System_printf ("Error: Unable to start the QMSS\n"); return -1; }
/* Memory Region 0 Configuration */ memRegInfo.descBase = (UInt32 *)l2_global_address((UInt32)host_region); memRegInfo.descSize = SIZE_HOST_DESC; memRegInfo.descNum = NUM_HOST_DESC; memRegInfo.manageDescFlag = Qmss_ManageDesc_MANAGE_DESCRIPTOR; memRegInfo.memRegion = Qmss_MemRegion_MEMORY_REGION_NOT_SPECIFIED;
/* Initialize and inset the memory region. */ result = Qmss_insertMemoryRegion (&memRegInfo); if (result < QMSS_SOK) { System_printf ("Error inserting memory region: %d\n", result); return -1; }
/* Initialize CPPI CPDMA */ result = Cppi_init (&cppiGblCfgParams); if (result != CPPI_SOK) { System_printf ("Error initializing Queue Manager SubSystem error code : %d\n", result); return -1; }
/* CPPI and Queue Manager are initialized. */ System_printf ("Debug(Core %d): Queue Manager and CPPI are initialized.\n", coreNum); System_printf ("Debug(Core %d): Host Region 0x%x\n", coreNum, host_region); return 0;}
/** * @b Description * @n * Application Raw Receive Cleanup API. * * @retval * Not Applicable. */static void myAppRawRxFree(Srio_DrvBuffer hDrvBuffer){ Qmss_QueueHnd returnQueueHnd;
/* Get the return queue. */ returnQueueHnd = Qmss_getQueueHandle(Cppi_getReturnQueue(Cppi_DescType_HOST, (Cppi_Desc*)hDrvBuffer));
/* Push the descriptor into the return queue. */ Qmss_queuePushDescSize (returnQueueHnd, (Ptr)hDrvBuffer, sizeof(Cppi_HostDesc));}
/** * @b Description * @n * This is the main DIO Example Task * * @retval * Not Applicable. */static Void dioExampleTask(UArg arg0, UArg arg1){ Qmss_QueueHnd myRxFreeQueueHnd; Qmss_QueueHnd myRxCompletionQueueHnd; Qmss_QueueHnd tmpQueueHnd; UInt32 numAllocated; UInt8 isAllocated; Cppi_DescCfg descCfg; UInt16 index; Cppi_HostDesc* ptrHostDesc; UInt8* ptrRxData; UInt32 numRxBuffers; Srio_DrvConfig appCfg; Srio_DrvConfig drvCfg; Qmss_Queue queueInfo;
/* Initialize the SRIO Driver Configuration. */ memset ((Void *)&appCfg, 0, sizeof(Srio_DrvConfig)); /* Initialize the SRIO Driver Configuration. */ memset ((Void *)&drvCfg, 0, sizeof(Srio_DrvConfig));
/* Initialize the OSAL */ if (Osal_dataBufferInitMemory(SRIO_MAX_MTU) < 0) { System_printf ("Error: Unable to initialize the OSAL. \n"); return; }
/******************************************************************************** * The SRIO Driver Instance is going to be created with the following properties: * - Application Managed * - Receive Completion Queue is Application specified; which implies that there * is no interrupt support. Applications will hence need to poll the queue to * check if there is data available or not. * - The Receive Free Descriptor Queues along with the Size thresholds are * managed and created by the application. ********************************************************************************/ /* Create the application receive free queue. */ myRxFreeQueueHnd = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated); if (myRxFreeQueueHnd < 0) { System_printf ("Error: Unable to create application receive queues.\n"); return; }
/* Create the application receive completion queue. */ myRxCompletionQueueHnd = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated); if (myRxCompletionQueueHnd < 0) { System_printf ("Error: Unable to create the application receive completion queue.\n"); return; }
/* Debug Message: */ System_printf ("Debug(Core %d): AppConfig RxFreeQueue: 0x%x RxCompletionQueue: 0x%x\n", coreNum, myRxFreeQueueHnd, myRxCompletionQueueHnd);
/* We are going to be using 4 receive buffers in this example. */ numRxBuffers = 4;
/* Application created queue which stores all the receive buffers. */ descCfg.memRegion = Qmss_MemRegion_MEMORY_REGION0; descCfg.descNum = numRxBuffers; descCfg.destQueueNum = QMSS_PARAM_NOT_SPECIFIED; descCfg.queueType = Qmss_QueueType_GENERAL_PURPOSE_QUEUE; descCfg.initDesc = Cppi_InitDesc_INIT_DESCRIPTOR; descCfg.descType = Cppi_DescType_HOST; descCfg.returnQueue = Qmss_getQueueNumber(myRxFreeQueueHnd); descCfg.epibPresent = Cppi_EPIB_NO_EPIB_PRESENT; descCfg.returnPushPolicy = Qmss_Location_HEAD; descCfg.cfg.host.returnPolicy = Cppi_ReturnPolicy_RETURN_ENTIRE_PACKET; descCfg.cfg.host.psLocation = Cppi_PSLoc_PS_IN_DESC; tmpQueueHnd = Cppi_initDescriptor (&descCfg, &numAllocated); if (tmpQueueHnd < 0) { System_printf ("Error: Unable to create application receive queues.\n"); return; }
/* Initialize the application receive buffers. */ for (index = 0; index < descCfg.descNum; index++) { /* Pop off a descriptor */ ptrHostDesc = (Cppi_HostDesc *)Qmss_queuePop(tmpQueueHnd); if (ptrHostDesc == NULL) return; /* Allocate the receive buffer where the data will be received into by the SRIO CPDMA. */ ptrRxData = (UInt8*)Osal_srioDataBufferMalloc(SRIO_MAX_MTU); if (ptrRxData == NULL) return;
/* Set the DATA and ORIGNAL DATA in the buffer descriptor. */ Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc*)ptrHostDesc, (UInt8*)ptrRxData, SRIO_MAX_MTU); Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc*)ptrHostDesc, (UInt8*)ptrRxData, SRIO_MAX_MTU);
/* Add the packet descriptor to the Application Receive Free Queue. */ Qmss_queuePushDescSize (myRxFreeQueueHnd, (UInt32*)ptrHostDesc, SIZE_HOST_DESC); }
/* Close the temporary queue. */ Qmss_queueClose (tmpQueueHnd);
/* Setup the SRIO Driver Configuration: This is application managed configuration */ appCfg.bAppManagedConfig = TRUE;
/* Get the queue information about the receive completion queue. */ queueInfo = Qmss_getQueueNumber(myRxCompletionQueueHnd);
/* The application managed configuration is capable of reception. */ appCfg.u.appManagedCfg.bIsRxFlowCfgValid = 1;
/* Configure the Receive Flow */ appCfg.u.appManagedCfg.rxFlowCfg.flowIdNum = -1; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_qnum = queueInfo.qNum; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_qmgr = queueInfo.qMgr; appCfg.u.appManagedCfg.rxFlowCfg.rx_sop_offset = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_ps_location = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_desc_type = 0x1; /* Host Descriptor. */ appCfg.u.appManagedCfg.rxFlowCfg.rx_error_handling = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_psinfo_present = 0x1; /* PS Information */ appCfg.u.appManagedCfg.rxFlowCfg.rx_einfo_present = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_tag_lo = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_tag_hi = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_src_tag_lo = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_src_tag_hi = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_tag_lo_sel = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_dest_tag_hi_sel = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_src_tag_lo_sel = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_src_tag_hi_sel = 0x0;
/* Disable Receive size thresholds. */ appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh0_en = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh1_en = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh2_en = 0x0;
/* Use the Application Receive Free Queue for picking all descriptors. */ queueInfo = Qmss_getQueueNumber(myRxFreeQueueHnd); appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq1_qnum = queueInfo.qNum; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq1_qmgr = queueInfo.qMgr; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq2_qnum = 0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq2_qmgr = 0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq3_qnum = 0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq3_qmgr = 0;
/* Use the Receive Queue for picking the SOP packet also. */ appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz0_qnum = queueInfo.qNum; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz0_qmgr = queueInfo.qMgr;
/* There are no size thresholds configured. */ appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh0 = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh1 = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_size_thresh2 = 0x0;
/* The other threshold queues do not need to be configured */ appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz1_qnum = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz1_qmgr = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz2_qnum = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz2_qmgr = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz3_qnum = 0x0; appCfg.u.appManagedCfg.rxFlowCfg.rx_fdq0_sz3_qmgr = 0x0;
/* Polling Mode: So dont program the accumulator. */ appCfg.u.appManagedCfg.bIsAccumlatorCfgValid = 0;
/* Populate the rest of the configuration. */ appCfg.u.appManagedCfg.rawRxFreeDrvBuffer = myAppRawRxFree; /* Start the application Managed SRIO Driver. */ hAppManagedSrioDrv = Srio_start(&appCfg); if (hAppManagedSrioDrv == NULL) { System_printf ("Error(Core %d): Application Managed SRIO Driver failed to start\n", coreNum); return; }
/******************************************************************************** * The SRIO Driver Instance is going to be created with the following properties: * - Driver Managed * - Interrupt Support (Pass the Rx Completion Queue as NULL) ********************************************************************************/ /* Setup the SRIO Driver Managed Configuration. */ drvCfg.bAppManagedConfig = FALSE;
/* Driver Managed: Receive Configuration */ drvCfg.u.drvManagedCfg.bIsRxCfgValid = 1; drvCfg.u.drvManagedCfg.rxCfg.rxMemRegion = Qmss_MemRegion_MEMORY_REGION0; drvCfg.u.drvManagedCfg.rxCfg.numRxBuffers = 4; drvCfg.u.drvManagedCfg.rxCfg.rxMTU = SRIO_MAX_MTU; /* Accumulator Configuration. */ { int32_t coreToQueueSelector[4];
/* This is the table which maps the core to a specific receive queue. */ coreToQueueSelector[0] = 704; coreToQueueSelector[1] = 705; coreToQueueSelector[2] = 706; coreToQueueSelector[3] = 707;
/* Since we are programming the accumulator we want this queue to be a HIGH PRIORITY Queue */ drvCfg.u.drvManagedCfg.rxCfg.rxCompletionQueue = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE, coreToQueueSelector[coreNum], &isAllocated); if (drvCfg.u.drvManagedCfg.rxCfg.rxCompletionQueue < 0) { System_printf ("Error: Unable to open the SRIO Receive Completion Queue\n"); return; }
/* Accumulator Configuration is VALID. */ drvCfg.u.drvManagedCfg.rxCfg.bIsAccumlatorCfgValid = 1;
/* Accumulator Configuration. */ drvCfg.u.drvManagedCfg.rxCfg.accCfg.channel = coreNum; drvCfg.u.drvManagedCfg.rxCfg.accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL; drvCfg.u.drvManagedCfg.rxCfg.accCfg.queueEnMask = 0; drvCfg.u.drvManagedCfg.rxCfg.accCfg.queMgrIndex = coreToQueueSelector[coreNum]; drvCfg.u.drvManagedCfg.rxCfg.accCfg.maxPageEntries = 2; drvCfg.u.drvManagedCfg.rxCfg.accCfg.timerLoadCount = 0; drvCfg.u.drvManagedCfg.rxCfg.accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT; drvCfg.u.drvManagedCfg.rxCfg.accCfg.listEntrySize = Qmss_AccEntrySize_REG_D; drvCfg.u.drvManagedCfg.rxCfg.accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT; drvCfg.u.drvManagedCfg.rxCfg.accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE;
/* Initialize the accumulator list memory */ memset ((Void *)&gHiPriAccumList[0], 0, sizeof(gHiPriAccumList)); drvCfg.u.drvManagedCfg.rxCfg.accCfg.listAddress = l2_global_address((UInt32)&gHiPriAccumList[0]); }
/* Driver Managed: Transmit Configuration */ drvCfg.u.drvManagedCfg.bIsTxCfgValid = 1; drvCfg.u.drvManagedCfg.txCfg.txMemRegion = Qmss_MemRegion_MEMORY_REGION0; drvCfg.u.drvManagedCfg.txCfg.numTxBuffers = 4; drvCfg.u.drvManagedCfg.txCfg.txMTU = SRIO_MAX_MTU;
/* Start the Driver Managed SRIO Driver. */ hDrvManagedSrioDrv = Srio_start(&drvCfg); if (hDrvManagedSrioDrv == NULL) { System_printf ("Error(Core %d): SRIO Driver failed to start\n", coreNum); return; }
/* Hook up the SRIO interrupts with the core. */ EventCombiner_dispatchPlug (48, (EventCombiner_FuncPtr)Srio_rxCompletionIsr, (UArg)hDrvManagedSrioDrv, TRUE); EventCombiner_enableEvent(48);
/* Run the loopback data transfers on the system initialization core. */ if (coreNum == CORE_SYS_INIT) {#ifndef SIMULATOR_SUPPORT /* DIO is NOT supported on the simulator */
/* DIO Write Operation */ if (dioSocketsWithISR (hDrvManagedSrioDrv, Srio_Ftype_WRITE, Srio_Ttype_Write_NWRITE_R) < 0) { System_printf ("Error: Loopback DIO ISR example for Write operation failed\n"); Task_exit(); }
/* DIO Write Operation */// if (dioSocketsWithISR_Write (hDrvManagedSrioDrv, Srio_Ftype_WRITE, Srio_Ttype_Write_NWRITE_R) < 0)// {// System_printf ("Error: Loopback DIO ISR example for Write operation failed\n");// Task_exit();// } /* Reset global counters before next run */// srioDioLsuGoodTransfers = 0;// srioDioLsuBadTransfers = 0;
/* DIO Read Operation */// if (dioSocketsWithISR_Read (hDrvManagedSrioDrv, Srio_Ftype_REQUEST, Srio_Ttype_Request_NREAD) < 0)// {// System_printf ("Error: Loopback DIO ISR example for Read operation failed\n");// Task_exit(); // }#endif }
/* Print out the Malloc & Free Counter */ System_printf ("Debug(Core %d): Allocation Counter : %d\n", coreNum, malloc_counter); System_printf ("Debug(Core %d): Free Counter : %d\n", coreNum, free_counter);
/* Check if there is a memory leak? Since we dont implement a 'deinit' API we need to * be careful in these calculations * - For the Application Managed Driver Instance * There will be 'numRxBuffers' + 1 (Driver Instance) * - For the Driver Managed Driver Instance * There will be 'numRxBuffers' + 'numTxBuffers' + 1 (Driver Instance) * Take these into account while checking for memory leaks. */ if ((numRxBuffers + 1) + free_counter + (drvCfg.u.drvManagedCfg.rxCfg.numRxBuffers + drvCfg.u.drvManagedCfg.txCfg.numTxBuffers + 1) != malloc_counter) { System_printf ("Error: Memory Leak Detected\n"); Task_exit(); }
/* Control comes here implies that example passed. */ System_printf ("Debug(Core %d): DIO with Interrupts example completed successfully.\n", coreNum); Task_exit();}
/** * @b Description * @n * Entry point for the example * * @retval * Not Applicable. */Void main(Void){ Task_Params taskParams;
/* Get the core number. */ coreNum = CSL_chipReadReg (CSL_CHIP_DNUM);
#ifdef SIMULATOR_SUPPORT#warn SRIO DIO LSU ISR example is not supported on SIMULATOR !!! System_printf ("SRIO DIO LSU ISR example is not supported on SIMULATOR. Exiting!\n"); return;#else System_printf ("Executing the SRIO DIO example on the DEVICE\n");#endif
#ifdef TEST_MULTICORE /* Initialize the heap in shared memory. Using IPC module to do that */ Ipc_start();#endif
/* Initialize the system only if the core was configured to do so. */ if (coreNum == CORE_SYS_INIT) { System_printf ("Debug(Core %d): System Initialization for CPPI & QMSS\n", coreNum);
/* System Initialization */ if (system_init() < 0) return; /* Power on SRIO peripheral before using it */ if (enable_srio () < 0) { System_printf ("Error: SRIO PSC Initialization Failed\n"); return; } /* Device Specific SRIO Initializations: This should always be called before * initializing the SRIO Driver. */ if (SrioDevice_init() < 0) return;
/* Initialize the SRIO Driver */ if (Srio_init () < 0) { System_printf ("Error: SRIO Driver Initialization Failed\n"); return; }
/* SRIO Driver is operational at this time. */ System_printf ("Debug(Core %d): SRIO Driver has been initialized\n", coreNum);
/* Write to the SHARED memory location at this point in time. The other cores cannot execute * till the SRIO Driver is up and running. */ isSRIOInitialized = 1;
/* The SRIO IP block has been initialized. We need to writeback the cache here because it will * ensure that the rest of the cores which are waiting for SRIO to be initialized would now be * woken up. */ CACHE_wbL1d ((void *) &isSRIOInitialized, 128, CACHE_WAIT); } else { /* All other cores need to wait for the SRIO to be initialized before they proceed. */ System_printf ("Debug(Core %d): Waiting for SRIO to be initialized.\n", coreNum);
/* All other cores loop around forever till the SRIO is up and running. * We need to invalidate the cache so that we always read this from the memory. */ while (isSRIOInitialized == 0) CACHE_invL1d ((void *) &isSRIOInitialized, 128, CACHE_WAIT);
/* Start the QMSS. */ if (Qmss_start() != QMSS_SOK) { System_printf ("Error: Unable to start the QMSS\n"); return; }
System_printf ("Debug(Core %d): SRIO can now be used.\n", coreNum); }
/* Create the DIO Example Task.*/ Task_Params_init(&taskParams); Task_create(dioExampleTask, &taskParams, NULL);
/* Start the BIOS */ BIOS_start();}