This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO DirectIO from/to DDR?



Hi,

I'm new to SRIO. Can the DirecIO (an external FPGA, for example), read/write directly to the DDR, without using the nulticore navigator?

I'm looking at the PDK examples but they use CPPI and SYS/BIOS. There is somewhere a minimalistic but complete example for DirectIO configuration that don't use SYS/BIOS?

  • Hello Alberto,

     

    I'm looking up the SRIO User Guide right now and hope to have an anwser for you real shortly.

     

    Thanks

    Elush Shirazpour

  • Alberto,

     

    The SRIO Direct IO does not need the multicore navigator to send/recieve data. The CPPI, or multicore navigator, is independent of the SRIO Direct IO. For Direct IO transmit operations, the user needs to work with the LSU shadow registers.

    You can access the SRIO User Guide at http://www.ti.com/lit/ug/sprugw1a/sprugw1a.pdf to look up examples.

     

    If I have anwsered your question, please click the Verify Answer button on the bottom of this post.

     

    Thank you

    Elush Shirazpour

  • Hi,

    Thanks, you confirm my interpretation of the srio user guide, but my real problem is if it can write/read to L2 only or also to DDR. Looking on sprigw1 overview ant block diagram it seems it is connected to L2 only (that include L2SRAM and MCSM)

  • Alberto,

     

    The DDR communicates with the TeraNet Switch Fabric through the MSMC. So the SRIO will have to communicate with the TeraNet to the MSMC to the DDR.

     

    Thank you

    Elush Shirazpour 

  • Alberto,

     

    To go into further detail, the SRIO can not communicate directly with the DDR.

     

    Thanks
    Elush Shirazpour

  • So, to summarize:

    1. with SRIO DirectIO from an external device (e.g. FPGA) I can write/read only to L2SRAM and also to  MCSM (4 Megabytes) For instance, a destination address 0x0C000000 will result in a transfer from FPGA to MCSM.

    If I use a doorbell to signal the end of transfer, when the doorbell arrives all previous SRIO tranfer are already completed and It is possible to immediatly launch an EDMA to transfer from MCSM to DDR.

    2. To operate on the DDR, I have to send SRIO messages (up to 16 SRIO packets per transactoin) on a Multicore Navigator queue and then I can move automatically to DDR by proper programming the multicore navigator.

    Is that correct?

  • Hello Alberto,

    You are correct in both terms, but let me clarify. The architecture of the Nyquist shows that any message goes to the MCSM, but you do not have to program the MCSM to send data to the DDR3. You can have your program send data from SRIO "directly" to the DDR3 and the complier will generate code in which it goes to the MCSM to the DDR.

     

    I hope I didn't confuse you before, but I thought you were asking the previous questions in terms of architecture.

    So to summarize...

    Archiecture: All packets go to the MCSM first and then the MCSM routes it to the DDR

    Programming: You can have your code send data directly to DDR and not worry about the MCSM

     

    Is that clear?

     

    Thank you

    Elush Shirazpour

  • Well, I'm still a bit confused. Just to say it in pratical terms, my question is: can an external FPGA write directly to the DSP DDR3 by sending an SRIO DirectIO packet (NWRITE) with desitnation address 0x80000000, without DSP CPU intervention ?

    I interpret your last message as a "yes": the SRIO "write" to the MCSM that route the writes to the DDR, and  this "routing" doens't  require any special setup by the CPU.

  • Alberto,

     

    Your intrepretation is correct. I didn't mean to confuse you before.

     

    Thank you

    Elush Shirazpour

     

    If I have anwsered your question, please click the Verify Answer button on the bottom of this post.

     

  • Alberto,

    i think you should try having your fPGA write to a DDR address. My fpga writes to 0x80000000 all the time and then sends a doorbell.  Search for my name and srio to find a lot of posts that go over this.

    on the other if you want the dsp to send out a dio message, you do have to have in l2 or msmcsram for the Lsu to work.

    brandy

  • BrandyJ said:

    i think you should try having your fPGA write to a DDR address. My fpga writes to 0x80000000 all the time and then sends a doorbell.  Search for my name and srio to find a lot of posts that go over this.

    Thanks, I'll look for.

    on the other if you want the dsp to send out a dio message, you do have to have in l2 or msmcsram for the Lsu to work.

    I did a very simple test program that, internal loopback core 0 only, send (NWRITE) from L2SRAM to DDR and then from DDR to L2SRAM. At first glance both works, while, If I understand, You say it should not work from DDR.

    I haven't yet tested with READ, but I suppose that if write works, read works also.

  • Alberto,

     

    For more detailed information, try looking at this E2E: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/215645.aspx

     

    Thanks

    Elush