Hi, All
My board have two C6678 communicate with a switch, It is working OK in 1.25G and 2.5G(4x mode), but it does not work with high speed (3.125G and 5G).The Port_OK bit is always 0 when I read SPn_ERR_STAT Register. My refclk is 156.25Mhz, the basic configuration of the register is as following(3.125G):
SRIO_SERDES_CFGPLL: 0x051 //pllMpy= 10;
SRIO_SERDES_CFGRX[0]:0x440495 //rate =2b'01
SRIO_SERDES_CFGRX[1]:0x440495
SRIO_SERDES_CFGRX[2]:0x440495
SRIO_SERDES_CFGRX[3]:0x440495
SRIO_SERDES_CFGTX[0]:0x180795
SRIO_SERDES_CFGTX[1]:0x080795
SRIO_SERDES_CFGTX[2]:0x080795
SRIO_SERDES_CFGTX[3]:0x080795
Is there any way to solve the problem, do I need to do some other configure for high speed transmission?
Many Thanks
Yang