Hi TI employee
We have an application to boot c6657 with nand flash. The hardware is the same with the 6657 EVM board.
Since we have the experience to boot c66x with spi norflash, we know that some init boot parameter should be loaded into nand first(we will not use i2c boot, so it must begin from block0).The problem is that we don't know what the format of parameter table is.We also don't know if we need some tool (like romparse.exe) to change it to some other file.
Can you give us some example parameter table and the code to write it into block0?
Does the parameter and the application code loaded into nand separately or together as a file?(We have found the example in mcsdk/tools/boot_loader/../nand_writer, but it seems like to load app code only.