Question from customer:
#1 In the SRIO multicore example program. How might I change it to use 8 cores instead of 4? What would need to change in the driver configuration?
I have attempted varying the amount of cores. 2-4 cores I have no issues with. Beyond that I have the first 4 cores start up fine then the rest display "Error: SRIO Driver Start Failed".
I have assigned new ID's for the remaining cores following the example.
#2 Does SRIO assume 4 1x lane ports by default? I do not see where in the initialization the port configuration occurs.