Hi,
I get kernel from MCSDK: mcsdk_linux_3_00_03_15;
In the kernel I find module: /lib/modules/3.10.10/extra/hplibmod.ko,
I need to insmod hplibmod.ko to kernel, but find following error:
hplibmod: disagrees about version of symbol module_layout
Error: could not insert module hplibmod.ko: Invalid module format
I understand the module is compiled with same version as kernel (since there are in the same SDK packet), why there is version verification error? How can I insmod hplibmod.ko without re-comliling module and kernel?
I get module and kernel information:
root@keystone-evm:/lib/modules/3.10.10/extra# modinfo hplibmod.ko
filename: /lib/modules/3.10.10/extra/hplibmod.ko
license: GPL v2
description: TI HPLIB kernel module.
author: Texas Instruments Incorporated
depends:
vermagic: 3.10.10 SMP mod_unload modversions ARMv7 rt-patch
parm: memSize:Size of DMA coherent memory to be allocated (uint)
root@keystone-evm:/lib/modules/3.10.10/extra# uname -r
3.10.10
I try modprobe -f hplibmod.ko, it does not work either.
Thank you very much!