hi,
In order to communicate between CORES Multicore Navigator must need or Message Queues are enough to create the communication between the cores.
Thanks
sri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
In order to communicate between CORES Multicore Navigator must need or Message Queues are enough to create the communication between the cores.
Thanks
sri
Hi Sridharan paneer83,
MessageQ are sufficient to communicate between the cores.
Please find the significant difference between the Multicore Navigator and Message Queues.
Multicore Navigator is a generic routing mechanism which can offload the work of the cores. The Multicore Navigator can be used for three type of tasks:
• Peripherals routing
• Interdevice communication (data movement, messages, synchronization)
• Dynamic load optimization between cores
Message Queues: -
One of the modules of IPC is MessageQ.
Inter-Processor Communication (IPC) provides a processor-agnostic API which can be used for communication between processors in a multi-processor environment (inter-core), communication to other threads on same processor (inter-process), and communication to peripherals (inter-device).
For more info, please visit, http://processors.wiki.ti.com/images/4/42/NavigatorForDummy_TP2.pdf
http://processors.wiki.ti.com/index.php/IPC_User%27s_Guide
Regards,
Shankari
Hi Sri,
For Multicore Navigator, please refer to the following links:
http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#Queue_Manager_.28QMSS.29
http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#QMSS_IPC_Transport
http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#IPC_QMSS_Transport_Message_Passing
http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#QMSS.2FNavigator_IPC_Transport
For Message Queues, refer to the ipc lab ppts at
http://processors.wiki.ti.com/index.php/IPC_3.x#IPC_Training
Regards,
Shankari
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------