Hi,
I had a query regarding the low priority accumulation queues.
I am using c6670 , now I want to enable low priority accumulation for 4 queues(I understand upto 32 queues can be monitored this way, I want just 4).
Now each queue is supposed to belong to different cores, s in case say I push a descriptor with psinfo containing the core number, I want to check this in the ISR which will be called in all cores. Depending on the core number I will either execute the required functionality on a particular core otherwise I will return from that particular ISR.
What I wanted to confirm is, do I have to acknowledge and EOI on each core separately?
I understand that I need to map this accumulator channel event number corresponding to low priority to a interrupt vector id which is unique 12 interrupt for all the cores. So it seems I need to acknowledge the interrupt on all the core?
Is my understanding correct so far.
Thanks in advance.