Hi Support,
Test case is like 1 DSP "C6638" communicating with other DSP "C6482" over SRIO Switch.
I am simulating a test case where a routing table entry is missing such that transaction timeout will occur.
My observation is that after certain transactions the LSU status is FULL and remains that only.
I have tried to do the LSU flush, restart, cancel with the required privID "core0 = 0" but nothing has worked.
I am avoiding the SRIO reinitializing as the C6638's 8 cores will have a respective LSU and the cores working is independent of each other.
How can I free my LSU and start working normally.
Regards,
Manav