I am bring up SRIO link between the Vertex 7 (vc707) and FMC667 (6678) daughter card. Our base line is from C:\ti\pdk_C6678_1_1_2_6\packages\ti\drv\srio\test\tput_benchmarking project. We were able to get SRIO port 0 to connect between the FPGA and DSP after hard coding the SRIO PLL value to 0x229 and rx/txConfig to 0x00440485. We had to make these change to get the 6678 DSP with core clock of 1.25MHZ to lock the PLL when using the FMC667 250MHz SRIO Ref clock. Now we are having problems with receiving Type 11 message with a size of 256B from the FPGA (We are running the DSP in polling mode). We have verified the FPGA can decode Type-11 message from the DSP with its SRIO IP. We are using x4 port configuration and 16-bit Src/Dest Ids. We noticed that for messages coming out the FPGA that the start of the message header is on lane 1 versus the messages coming out the DSP message header starts on lane 0. Could this cause alignment problem with SRIO decoder on the 6678?