Hi
Our research faced a problem that when 6678 DSP(evm6678) is programmed in the PLL MODE, which is working at 1GHz. It cannot talk with other 6455 DSP through SRIO switches. At first, we leave the PLL in by-pass mode. 6678 can talk with other 6455 through two SRIO switches in the 100MHz. However, when 6678 is programmed at 1GHz, 6788 cannot talk with 6455. In this scenario, 6678 can read and write the looped back packages from its own by switch.
Can anyone explain why this happen?
Thanks
Xining