Hi!
We use the SRIO interface in DSP tms320c6678. Now we see the processor is configured to SRIO with errors – configuration in a mode 1x instead required 4x. We see this errors at different speeds (2.5 Gb/s and 3.125 Gb/s).
We found out in the process of debugging that the lines "0" and "3" are not working correctly, other ones (lines "2" and "3") - incorrectly. We used an oscilloscope to test the lines. You can see in the first picture a wrong signals. It is a parasitic amplitude signal modulation with a period of 30-33 ns.
You can see in the second picture two signals simultaneously - correct and incorrect.
Pic. 3 - configuration pf port is ok.
Pic. 4 - also ok.
Could you pls help us to find the bug?
Thanks