Good day to you again. The last thing i'm trying to do with my tmdsevm6670l is making on-board calculation. So, if i'm right, i must do the further algorhytm:
- Boot the board with ethernet boot mode;
- Use the program (changed "client" project in my case) to initialize the DHCP server and make the board to "answer" to ping;
- This programm also must hold 2 ethernet buffers: for receiving data from PC and for sending it back to it (i can't load another, because of memory config, i don't know why this is happening, but this is really sad thing);
- I have to send the packets with data for calculation for the bufer with specific memory range, board must read this data, calculate it, write to the send buffer and then send it back.
I've searched in NDK documents and found the information about sockets, but i did not quite understand the mechanism of their creation. Also, how do I set a specific address for those buffers? And also, maybe i did not even need socket connection?
With best regard, Taras.