Hi,
I tried to get the H265venc_ti_c66x project running in CCS 6.1 on my EVMK2HX board. In order to get it linked, I replaced ERAM in h265venc.cfg with DDR3, after that the MSMCSRAM was still overflowing because it was all used up by the .SL2_mem. What makes me wonder is why the MSMCSRAM has a size of 0x200000 in the linker, when the actual hardware has 6144k? Anyway, I then moves SL2_mem to DDR3 as well. Unfortunately that appears to be a bad idea because the program crashes at the VidMc_Init function during initialisation.
So I am wondering, I can't possibly be the first to get this codec running on the AK2H right? Could anyone help me with their project to get started?
Or should I switch to CCS5.5 with the MCSDK_Video?