Hi,
My customer is planing to design their target board with K2H. To do this, they are trying to understand the current K2H EVM schematic.
I'm just looking at :
Please refer Microcontroller Block Diagram at page 9.
Now some questions:
- What is the purpose of the UART connection between MCU and K2H ? Can I understand this is a bus for sending LCD information data (IP address) from K2H to MCU ?
- I2C0 on K2H is connected to I2C1 on MCU. Is this used to access MCU registers from K2H side in runtime ? If yes, what is the main purpose for ?
- Also, this I2C bus is connected to EEPROM and UCD9090. From my understanding, K2H would be a bus master to EEPROM (read and write) and the connection between MCU and EEPROM is just reserved option. And as for UCD9090, the main control bus (UCD9090 programmer) would be PMBUS via Fusion software and MCU would do nothing for UCD9090 in runtime. MUC would monitor POWER GOOD status of UCD9090 in order to control K2H reset signals (like POR, RESETFULL, etc...) via IO expander. Correct ?
- I2C1 on K2H is connected to Microchip IO expander (SPI to GPIO). Is this used to access K2H from MCU side in runtime ? If yes, what is the main purpose for ?
Best Regards,
Naoki