Hi
CCSv5
C6000_cgt_7.4.15
C++
I've added the IQMath 2.1.4.0 library to my C++ C6678 folders and added the folder to the include path.
I've added the pre-processor define _INLINE_IQMATH
And this is how I've include the header files
#ifdef _INLINE_IQMATH
#include "IQmath_inline_all.h"
#else
#include "IQmath.h"
#endif
I get a ton of _abs errors and others. Basically any intrinsic in the IQMath_inline_all.h file.
Description Resource Path Location Type
Function '_abs' could not be resolved IQmath_inline_all.h /C6678_SeperateCfgPrj/IQMath_2_1_4_0/include line 697 Semantic ErrorFunction '_hill' could not be resolved IQmath_inline_all.h /C6678_SeperateCfgPrj/IQMath_2_1_4_0/include line 1094 Semantic Error
Any thoughts on how to fix the compiler errors?
Cheers2u
Eddie