Hi,
I have set my C6670 to bootload from NAND storage using IBL. This involved first setting IBL up via EEPROM and then flashing the image to NAND storage. I currently have a simple hello world image running.
I would like to bootload a single image on all 4 cores of my C6670. I have prepared an image, where based on the core number (i.e. DNUM), the value written to a variable is different. This way, I can tell that each core has loaded the image and is running it independently.
I was wondering if someone could walk me through what I would need to do to load this image on all 4 cores of my C6670 using this NAND-IBL setup. I came across the MAD utilities while searching, but it seemed too complicated for loading just a single image on all cores (rather than different images on each core). I have seen discussions around this, but haven't really encountered a working solution.
Thank you for your help!