We are using the K2G on the evmK2G.
The DCAN0_TX pin toggles external when programmed via GPIO.
I did write a DCAN0 test which passes when I turn on internal loop with or without silent mode.
I do not see a signal toggling on the DCAN0_TX pin (in non silent mode).
The test fails when external test mode is turned on.
When I switch off loop testing, I still don’t see activity on the DCAN0_TX pin.
I measure with a nice osci (DCAN0_TX pin to GND) with and without an external 120R.
I see the behavior on both of our evmK2G boards.
What am I doing wrong ?
Thank you for your time in advance.