Hi,
Based on the K2L EVM, its recommeded to use 1.0V for CVDD1, is it correct? But on 66AK2L06 datasheet, its stated should use 0.95V for CVDD1 (page 215), on page 212 its recommended to use 1.0V (nominal) for cvdd1, which one is correct? is the 66AK2L06 able to turn on if i using 1.0V for CVDD1? Currently i follow the same power sequencing as stated in the EVM board but my board still not able to bootup, could you please help on this? Thanks.