Other Parts Discussed in Thread: SYSBIOS
Hello,
We are working on udp on ethernet link and we see following behaviour:
-Everything seems to go OK as long as we have small packet to send smaller than 1400 Bytes
-From the moment we have to send larger packets (multiply time 1400 Bytes after each other) we are in trouble only in case we have enabled some other sampling (based on high rate interrupt ) routine enabled.
-This sampling routine (the interrupts works fine) on his own.
With in trouble I mean the system crashes after some time. After some debugging I remember we enabled ti.sysbios.family.c64p.Hwi instead of the standard hwi module.
This in order to be able to mask interrupt. However we stay for ethernet with the example provided by TI.
Then I did some research on the internet and came across following topic:
https://e2e.ti.com/support/embedded/tirtos/f/355/p/503663/1829170#
which seems for me on a first glance the same problem.
Is following true? By using maskable interrupt you missing events coming from the ethernet device. This need to be catched in some way?
Is it possible to use the ti.sysbios.family.c64p together with ethernet udp?
Best regards.