Tool/software: Linux
Hello
I'm have a problem with USB 3.0 port using on EVMK2H Rev 3.0 board. My final target is to use USB sound card to capture audio stream. I'am using the last version of Arago, that included in TI Processor SDK (kernel version Linux k2hk-evm 4.9.28). The execution result of lsmod and dmesg command shows, that all necessary kernel modules such as usb_core, usb_common, xhci_hcd was succesfully launched. But every time, when i try to connect any USB device (usb flash drive, usb sound card, usb modem, etc), power LED on device is not active, and lsusb show only root hub's in the device list. Besides, there was only one time, when USB port was power on, and LED was active. I'd suppose, that it seems to be a random event. In any other time there is no power on USB port. Previously, when i've prepared my workstation, i had tried to use boot USB drive, and the USB port was active only one time on approx 20 tries. I think, it seems as software problem, maybe it's not unusual and you could recommend me some ways to solve it?
Best regards,
Nikolay