Hello Team,
Posting on behalf of customer:
I have seen differing advice on the termination of the DDRRESET line from the TMS320C6678. On one reference design it is pulled up to VTT on another it is pulled up to 1.5V and on the Keystone Wiki, it recommends pulling it down to GND. We currently have it implemented with DDRRESET pulled up to VTT.
During normal operation the DDRRESET line was only getting to 0.5V. To test if the TMS320C6678 is actively driving the line, I removed the pullup and noted that the line does not get driven high. Looking at the Micron Spec for the memory they recommend DDRRESET = 0.8 * VDD just like in one of the TMS320C6678 manuals.
I personally believe that the line should be pulled up to 1.5V. What is the factory recommendation, and why?
Thanks,
Keith N.
AFA OH/wPA