Tool/software: Linux
Hi. i use k2h board and processor sdk u-boot and kernel.
I want to build a nand.bin file (.ubi file) from my rebuilt kernel (zImage file) and device tree fils (.dtb) and some other files (skern-k2hk.bin and k2-fw-initrd.cpio.gz).
I used arago-console-image-k2hk-evm.tar.gz in MCSDK 3.01.04.07 and extract it. then copied these files in /boot.
with use of these two commands, i made an Ubi files:
sudo mkfs.ubifs -F -m 2048 -e 126976 -c 3970 -r ~/tisdk-server-rootfs-image-k2hk-evm tisdk-server-rootfs-image-k2hk-evm.img
ubinize -o tisdk-server-rootfs-image-k2hk-evm.ubi -m 2048 -p 128KiB -s 2048 -O 2048 ubinize.ini
ubinize file is:
[ubi_rfs]
mode=ubi
image=tisdk-server-rootfs-image-k2hk-evm.img
vol_id=0
vol_size=480MiB
vol_type=dynamic
vol_name=ubi_rfs
vol_flags=autoresize
but it didnt boot on my board.