Part Number: TCI6638K2K
Hi,
We want to interface TCI6638K2K with an eUSB module which is +3.3V with a 10pin header (having all the USB2.0 and USB3.0 signals and +3.3V power pin).
USBVBUS is a +5V, analog input for monitoring the voltage on VBUS. In this case the VBUS is 3.3V since the USB Device is +3.3V. So can we connect +3.3V to this pin instead of +5V in this case.
Please confirm.
Thanks and Regards,
Remya