Hi all,
We are trying to utilize the VPFE peripheral of the DM365 Video Processor, but we are facing some difficulties.
Looking at the ISIF block diagram we see a "16-to-12 Bit" block used to convert a 16-bit signal to 12-bit signal.
The above block is followed by a mux which is used to select between the output of this block and a another 12-bit signal (part of the input to the "16-to-12 Bit" block).
- How do we control the mux? The diagram has no indication for the select line.
- How does the second input to the mux look like? Is it the 12 LSB of the data?
Regards,
Holden