Hi all,
I am working on DVR RDK 4.0 and meet a displaying problem---field is incomplete.I read data from encoded file,then decode and display to test the interlace display,and find that field dispaly is incomplete,only one field.Did anyone met the problem?pls TI experts check this problem ,i will give the test file to you.
The h264 file was saved by capture&encode link in DVRRDK4.0 ,the input video resolution is 1080i60hz, you can find this h264 file in attachment 2465.error_test.rar,the file include 240 frames(480 fields) data,you can use Elecard StreamEye Tools to view the file in pc,and you will find the encode date has two different fields,one is black,the other is white,the image as follows: