For DM8107 or DM385, one can select separated values for several IO groups.
We are currently designing with DM8107 (very similar to DM385) and we plan to use a single 1.8V digital supply rail for all the IOs.
We also plan to use a single 1.35V supply rail for all core supplies (nitro mode).
We wonder how this affect the POH ?
Is the 1.8V best for POH or is worst than 3.3V for the IOs ?
If we have all IO rails under 1.8V, could we "skip" the 3.3V step in the recommended power up sequence ? (because the only remaining 3.3V supply only affects USB part)