Hi,
I would like to know whether two simultaneous Analog camera can be supported on DM385/DM383 with D1 resolution.We would use TVP5150 (2Ch decoder).
WHAT IF 4 CH IS USED. Can we as well have 4 simultaneous D1 camera interface.?
y2k
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, VIN port on DM385 actually supports TVP5150/TVP5158 as well.
What kind of product you want to develop? What interface/feature is required?
BR,
Eason
Hello Eason,
Thanks for the response. Product has two camera with D1 resolution. This can as well be used in CAR DVR POC. We dont need 1080p/720p. There are multiple applications. Question is whether we can really interface 2 cam to TVP5150/DM385 to get both camera stream for processing. We did not see any pixel muxing in this TVP5150.
How do we do this.
Y2K
Hi,
TVP5150 has 2 inputs but they are muxed to only 1 ADC. Which means TVP5150 is 1 ch decoder.
You can use 2 tvp5150 or 1 tvp5158.
BR,
Eason