Hi.
For JPEG encoder have a question.
Output image of jpeg encoder is broken, when qvalue is between 91 and 97.
I am looking for a solution to this problem.
Sdk environment that I have used is as follows.
・board: TMX320DM365 Digital Video Evaluation Module BETA
・sdk: ti-dvsdk_dm365-evm_4_02_00_06.
・application: dmai_2_20_00_15 image_encode_io1
Apllication command line args is as follows.
./image_encode_io1_dm365.x470MV -i /opt/sbin/random.yuv -c jpegenc -r 640x240 --qValue 97 --iColorSpace 3 --oColorSpace 2 -o demo.jpg -e encode
Input image is random noise image that high-frequency component is large.
Thanks for your help.