Hello,
I'm working with IPNC_RDK 5.1 SWOSD to display character strings on OLED for a camera.
The present SWOSD String Pattern has limited characters (77 characters). I would like to add more symbol characters. In accordance, i added the required symbols in SWOSD_STRINGPATTERN. I updated the YUV Database with the symbol image values as well. And as a final step, i changed the string width to be SWOSD_STRINGWIDTH_770_20 = 780 from the previous value 770 as the character width is 10. But when i try to display the new character symbols, the character display gets corrupted (DB gets corrupted). It works fine only for the present string pattern with string width 770 (i.e 77 characters).
I would be grateful if anyone could come up with the solution to this issue as soon as possible
Thanks