Hi,
My customer complained that the DM365 Jpegenc made the image blur (reduce the shapness) compared with original YUV or the jpeg file encoded by PC. So I want to try the file to file jpegenc sample code to check this issue.
I used the FC 2.4 and the other tools in ipnc 2.6 (kernel 2.6.18) and can build the jpgenc-r well. But when I run the app, it hangs in process call. I added the print info before and after the process call and I only see the print before process call is printed out.
With same environment, the h264dec sample code can work ok.
Would you pls kindly advise what I missed?
Below is the log info.
# ./jpgenc-r -ext
RMAN initialization done
VICP Protocol Registration Success
EDMA3 Protocol Registration Success
----- Running in extended parameter mode -----
Testcompliance = 0
Param file = ../TestVecs/Config/Testparams.cfg
Input file = ../TestVecs/Input/colorful_toys_cif_422ILE.yuv
Output file = ../TestVecs/Output/colorful_toys_cif.jpg
*******************************************
Read Configuration Set 1
*******************************************
Parameter file read starts...
Running in Output Dump Mode
Algorithm Instance Creation Done...
Number of Input bufs =1
status.imgencStatus.bufInfo.minInBufSize[0]=202752
number of bytes read from input file = 202752
Chris: Before process call