Other Parts Discussed in Thread: TMDSCSK388
Hello,
Basic on TMDSCSKCC + TMDSCSK388, follow the wiki step: http://processors.wiki.ti.com/index.php/IPNC_RDK_DM38x_,_DM8127
Using prebuilt binaries(sdcard or nand), in step 4 Running Application, I got the error about links_m3video:
[host]
Force IDR on Channel: 0
[host]
Force IDR on Channel: 1
[ 194.694641] autorun-usecase.sh[111]: [m3vpss ] 10642: DISPLAY: Start Done !!!
[ 194.706968] autorun-usecase.sh[111]: [m3vpss ] 10642: DISPLAY: SDDAC(SEC1): 833 fps, Latency (Min / Max) = ( 2 / 38 ), Callback Interval (Min / Max) = ( 31 / 34 ) !!!
[ 194.713729] autorun-usecase.sh[111]: [m3vpss ] 10461: VNF:
[ 194.717341] autorun-usecase.sh[111]: [m3vpss ] EnableSNF current SNF 1 => new 0!!!
[ 194.720127] autorun-usecase.sh[111]: [m3vpss ] NSF: EnableSNF 0 current mode 0!!!
[ 194.721076] autorun-usecase.sh[111]: [m3vpss ] 12115: VNF:
[ 194.721767] autorun-usecase.sh[111]: [m3vpss ] EnableTNF current TNF 1 => new 0!!!
[ 194.727264] autorun-usecase.sh[111]: [m3vpss ] NSF: EnableTNF 0 current mode 1!!!
[ 194.730864] autorun-usecase.sh[111]: [m3video] Channel:0 inputframerate:30 targetfps:30
[ 194.731852] autorun-usecase.sh[111]: [m3video] Channel:2 inputframerate:30 targetfps:5
[ 194.732548] autorun-usecase.sh[111]: [m3video] ENCLINK: new targetbitrate to set:10000000
[ 194.737399] autorun-usecase.sh[111]: [m3video] ENCLINK: new targetframerate to set:30000
[ 195.076988] autorun-usecase.sh[111]: [m3video] ENCLINK: new QP I Param to set:10 36 -1
[ 195.077577] autorun-usecase.sh[111]: [m3video] ENCLINK: new rate control algorithm to set:0
[ 195.078070] autorun-usecase.sh[111]: [m3video] Channel:1 inputframerate:30 targetfps:60
[ 195.078537] autorun-usecase.sh[111]: [m3video] JPGLINK: new QP Param to set:1 51 80
[ 195.079044] autorun-usecase.sh[111]: [m3video] 12593:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_jpeg.c:[89]::INTERNAL ERROR:-1
[ 195.079515] autorun-usecase.sh[111]: [m3video] ALGCONTROL FAILED:CMD:1
[ 195.079975] autorun-usecase.sh[111]: [m3video] 12593:WARN
[ 195.082960] autorun-usecase.sh[111]: [m3video] JPGLINK: ERROR in Run time parameters changes, Extended Error code:8192
I can see the HDMI output video stream a few seconds...after that, hdmi output became black screen.
Also, when run ./boot_proc 1& in autorun-usecase.sh, always got error: can not umount /mnt/mmc .
Thanks in advance.
Best regards
Dick