What latency can I expect doing H.264 encoding of a single stream of 720p @ 30fps (assume a 300MHz part)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What latency can I expect doing H.264 encoding of a single stream of 720p @ 30fps (assume a 300MHz part)?
Frank,
What latency are you refering to? I mean is it capture to display on DM365 or is it network latency from capture to encode to stream to PC decode? The answer would depend on that.
Have you referred to our IPNC Reference Design on DM365? That talks about different latencies. (www.ti.com/ipcamera)
Regards,
Anshuman
The latency I am referring to is capture to encode to displaying the video.
I was not able to find any latency information at the URL you provided. There is a brief description of the hardware and the capability to order the reference design but no latency information that I could find.
Thank you,
Frank
Hi,
What is the latency you are targetting? what is the end application you are using?
For IPNC we have arround less than 150ms as latency. This is complete system latency from sensor capture to PC display.
ALso, in codec, we support slice based encoding for low latency usecases.
Regards,
Raghu
Hello Raghu,
I can not tell you application as I am under NDA and also this is an open forum. But suffice it to say that this application can not have high latency. 150ms should be good.
What is IPNC mean? And can you elaborate on slice based encoding?
Thank you,
Frank
IPNC means IP Network Camera,
For slice based encoding you can look the H264 codec encoder datasheet.
But this slice based implementation will complicate the implementation.
So since 150ms is good enough, you suggest not to go ahead with slice based approach
Regards,
Raghu
I sent an email to customer to make sure that <150ms is tolerable for his application. But I believe it is.
Thank you for the explanatiion.
Hello Raghu,
What is the <150ms total latency time based on? Is it a canned demo with the eval kit? And what resolution is the video stream?
Thank you,
Frank
Raghu,
At the beginning of this train of requests for support, I mentioned that the customer was looking at using the DM365. So can you tell me what the complete latency is for that processor using H.264 encoding with a stream of 720p@30fps?
Thank you,
Frank
It is same for 720P@30fps i.e. <150ms .......
i mentioned 1080p as to say till max resolution for 30fps streaming.
Regards,
Raghu
Raghu Kudva said:It is same for 720P@30fps i.e. <150ms .......
i mentioned 1080p as to say till max resolution for 30fps streaming.
Regards,
Raghu
Mr Raghu,
At the beginning of this thread, the question was what latency can be expected, then changed to 150 msec is acceptable. I also looked at the link provided - it points to selling cameras. I thnk the original poser, and myself, would like to know how to achieve the 150 msec with our code and hardware. The H264 data sheet lists a few dozen parameters for the encoder, with pretty sparse descriptions of them. So let's try: Is there some reference material on using the parameters available in the H264 encoder, such as how to specify slices and the effect on latency. Network-related latency, we understand, is affected by the variable GOP size, requiring buffers to allow the average bit rate to be less than, say, the bit rate of I-Frames alone.
Thanks,
Arthur
HI,
What exactly the latency are you looking for?
You can look at the codec datasheet on how to use slice level encoding to achieve very low latency.
In the IPNC kit, we have it done on frame based encoding and we could achieve less than 150ms.
SO with slice based approach, you can still go lower but the system becomes very complex with slice mode operation.
Regards,
Raghu
Hi Raghu,
I have been using Custom made Leopard DM368.
We are getting 450ms for N/W video streaming Latency(capture+encode+n/w+decode+display). but our target is <150 ms. We have struk here almost two months.
By enabling Slicebase encoding We can achieve 280 ms. But you are telling without slicebase itself we can achieve 150ms.
Can you please Guide me to get <150ms Latency?
Regards,
Dasari