Hello!
For my project I need configure ISP pipeline like this:
sensor -> CCDC -> CCDC output
|
Resizer -> Resizer output
I use omap3-is driver from Linux-2.6.37
May be somebody did it. Please help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
For my project I need configure ISP pipeline like this:
sensor -> CCDC -> CCDC output
|
Resizer -> Resizer output
I use omap3-is driver from Linux-2.6.37
May be somebody did it. Please help me?
Hi,
I want that CCDC writes image data to Memory and Resizer.
After some manipulation with driver I did it.
But read from Resizer output possible only if other app reads from CCDC output.
I want that read was independent.
BR,
Michael
Hello Michael2:
My English is not good. I am so sorry for you to understand me.
I have a driver receive bt656 UYUV data . but it dose not use V4L2.
the driver modifies the registers directly ,
ccdc can writes image date to ccdc, and the resizer can be used also.
give me your mailbox and i send the code with test programe to you.
----------------------------------
I also meet a problem, I want receive VGA data and in the beginning i write a driver use v4l2 framework,
.interface = ISP_INTERFACE_PARALLEL,
.bus = {
.parallel = {
.data_lane_shift = 0,
//.vdpol=1,
.bridge =0x3,
but there is no VD0_IRQ , so i can not get image .
After that, I modified the driver which can receive bt656 data, I found if the CCDC_VDINT!=0, the VD0_IRQ will not generate.I can receive VD0_IRQ but the image is not right, only the fist line has date, other lines are all 0xffffffff.
I also found the ccdc state is alwsys busy.
8bit parallel data input , sensor -》 ccdc - > memory .
can you tell me what reason causes my error?
my mailbox is gaoshanv5@qq.com
Hello.
I need to do same thing on DM3730, kernel 2.6.37.
Idea is to have in memory video directly from CCDC on /dev/video2 and resized video on /dev/video6
I'm using media-ctl to create links for this.
When try to set output from CCDC to memory and to resizer it give me error that device is busy and that is expected because they are on same pad.
What modification you made in driver to achieve this?
How to change CCDC topology in driver to have CCDC output on different pad?
- entity 5: OMAP3 ISP CCDC (3 pads, 9 links)
type V4L2 subdev subtype Unknown
device node name /dev/v4l-subdev2
pad0: Input [UYVY 720x576]
<- 'OMAP3 ISP CCP2':pad1 []
<- 'OMAP3 ISP CSI2a':pad1 []
<- 'bt656_omap 3-005b':pad0 [ACTIVE]
pad1: Output [UYVY 720x576]
-> 'OMAP3 ISP CCDC output':pad0 [ACTIVE]
-> 'OMAP3 ISP resizer':pad0 []
pad2: Output [UYVY 720x575]
-> 'OMAP3 ISP preview':pad0 []
-> 'OMAP3 ISP AEWB':pad0 [IMMUTABLE,ACTIVE]
-> 'OMAP3 ISP AF':pad0 [IMMUTABLE,ACTIVE]
-> 'OMAP3 ISP histogram':pad0 [IMMUTABLE,ACTIVE]
Regards,
Vojislav
Hello Vojislav,
Sometime it's locking when open/close video stream.
Here is pipeline configuration:
media-ctl -v -r -l '"ov5640 2-003c":0->"OMAP3 ISP CCDC":0[1], "OMAP3 ISP CCDC":1->"OMAP3 ISP CCDC output":0[1]'
media-ctl -v -f '"ov5640 2-003c":0 [UYVY2X8 640x480], "OMAP3 ISP CCDC":0 [UYVY2X8 640x480], "OMAP3 ISP CCDC":1 [UYVY 640x480]'
media-ctl -l '"OMAP3 ISP CCDC VP":0->"OMAP3 ISP resizer":0[1], "OMAP3 ISP resizer":1->"OMAP3 ISP resizer output":0[1]'
media-ctl -f '"OMAP3 ISP CCDC VP":0[UYVY2X8 640x480], "OMAP3 ISP resizer":1[UYVY2X8 320x240]'