Hi all, I'm working with the DM3730 device and the resizer works well when I'm resizing the 720x576 video to the resolution of 720x288 and 352x288. But when I change it to 176x144 resolution, the output video is obviously not the correct resolution.
As is mentioned in 'AMDM37x Technical Reference Manual', the 1/16 resolution resizing process is supported:
"The resizer module can upsample or downsample image data with independent resizing factors in the horizontal and vertical directions. The HRSZ and VRSZ parameters can range from 64 to 1024 to give a resampling range from 4 to 0.25 (256/HRSZ or 256/VRSZ)."
So I'm wondering if there is something wrong with my configuration. The kernel version is 2.6.32.
Thanks,
Robert