Hello,
I'm using a C64+ containing in a DM3725.
In the Technical Reference Manual (AM/DM37x Multimedia Device Silicon Rev 1.x version R) it is said in chapter 5.4.4.1 that the EDMA optimizes transfers from/to the DSP megamodule memories to/from deviceon-chip and off-chip memories.
I would like to use EDMA with Hardware Trigger for UART1 and other devices. However when I look at the 5.2 table containing the request Mapping, I have no request for UART1. If I have a good comprehension of the table, I can only use EDMA for McBSPx and UART3, is it right ? if not , how can I use it for my purpose ?
Thank you very much for your help.
Regards.
Pat.