I managed make the D_CAN0 work s just fine. But I'm having trouble making D_CAN1 work. So far I have add resources for d_can1 in devices.c and called ti814x_d_can_init() for instance1. The loopback test works fine on dcan1, however when I connect the dcan port to a CAN device, it didn't work. (I did moved the jumpers to5-6 and 7-8 on CAN_SEL).
Has anyone ever made dcan1 work? Any comment/suggestion would be appreciated.
Jiewen