This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Christiano,
Do you have the TRM for TMDXIPCAM8127, that should give you the information for the peripheral set you mentioned.
Also, the IPNC RDK documentation and source code covers usage of -
However kernel drivers are included for USB and PCIe which should help you talk to these interfaces using standard Linux libraries.
Regards
Rajat
Hi Rajat,
Where can I find these TRMs? The Manuals in ti_tools/ipnc_psp_arago/docs it aren't complete enough.
Hi Rajat,
Where can I find these TRMs? The Manuals in ti_tools/ipnc_psp_arago/docs it aren't complete enough
Christiano,
The TRMs for processors are not released along with the software. Do you have any FAE/Sales contact in TI they can give it to you.
Regards
Rajat
Dear Rajat Sagar.
1. Does DM8127 support a usb wifi module by usb host mode ?
2. Can you recommend any commercial usb wifi dongle that works with DM8127 ?
Hi,
I am using DM8127 custom board. I am using UART1 port loopback ttyO1
echo "Hello" > /dev/ttyO1;cat /dev/ttyO1 nothing on output ??
BR
Tejas