Hi all:
My platform is dvr_rdk_4.1, when the vip0 (default) capture discrete syn vedio ,the height cant be recognized,
As this picture show:
DEMO: 0: Detected video at CH [0,0] (1280x720@60Hz, 0)!!!
[m3vpss ]
[m3vpss ] *** Capture Driver Advanced Statistics ***
[m3vpss ]
[m3vpss ] VIP Parser Reset Count : 0
[m3vpss ]
[m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Dropped Fid Repeat Frame Error Y/C
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C)
[m3vpss ] ------------------------------------------------------------------------------------------------------------
[m3vpss ] 000 | 1566 1 1565 3 0 3 1280 / 1280 5 / 5 1
The height only 5, actully it is 720.
When i change the capture embedded syn vedio mode, there only 1 field be captured.
The syn signal are Bt656 standard with data of 0xFF 0x00 ....
May bo something casuse to this phonomenon, in 816x it is ok with this vedio format.