Hi Guy...
We have developed product using DM388 that is based on IPNC EVB.
But we change default NAND device.(at IPNC EVB, Nand device is 16bit-2Gb).
in our product ,we use 8bit-2Gb Nand device.
The issue is that,
The Nand can read, write and verify under SD Boot.
When we set the boot_mode for nand boot,it cannot Nand boot. (It only shows “CCCCCC…” message).
The Nand part number is MX30UF2G28AB.
It's ID is Manufacturer ID: 0xc2, Chip ID: 0xaa (Macronix(MXIC) NAND 256MiB 1,8V 8-bit).
There may be something we have been missing.
We would deeply appreciate if you kindly help us.