Hi,
I'm currently have a diagnostings code in CCS5.5(linux) and i'm trying to run it from SD card.
Since this does a diagnostics, this will not load in the DDR of the board, will be in the Internal ram of the processor.
I have an MLO File And the U-Boot running for a kernel running from SD, but i'm not very sure which changes i have to do for using the other internal memory
The Diagnostics code has a GEL which is functional with the debugger, and that seems to do the Map of the pins. I would be grateful to have any reference, documentation, or any "how to start".
Thanks in advance